Posted by Andrew Zaske on Di, Okt 05 2021 @ 9:30

A pressing need

Electric servo-mechanical presses offer increased versatility and production improvement opportunities over hydraulic presses.

An electric servo-mechanical press offers all the versatility of a hydraulic press, with production speeds close to a flywheel press.

 

Comments (0)
Number of views (690)
Article rating: No rating

Posted by Ryan Klemetson on Di, Sep 07 2021 @ 9:30

In the bag

Design flexibility solves packaging problem

Rodless electro-mechanical actuators on a modular bagging system precisely position incoming bags regardless of size.

Comments (0)
Number of views (855)
Article rating: No rating

Posted by Andrew Zaske on Di, Aug 03 2021 @ 9:30

Gantry and multi-axis system: Build it your way

Follow a straight-forward four-step method

Gantries can be complicated and specialized. There are infinite variations for moving an object on multiple axes. But multi-axis motion control systems don’t have to be intimidating if you follow a straight-forward method that involves four steps. 

Comments (0)
Number of views (1640)
Article rating: No rating

Posted by Andrew Zaske on Di, Jul 06 2021 @ 9:30

Extend your reach

Linear actuators are the long arm for collaborative robots and autonomous guided vehicles

Actuators create the motion for collaborative robots and autonomous guided vehicles, whether it’s extending the reach of a robotic arm or steering a 40-foot shipping container. 

Comments (0)
Number of views (1039)
Article rating: No rating

Posted by Ryan Klemetson on Mi, Jun 02 2021 @ 9:30

Go electric!

Plug in to electromechanical actuators for new—and better—performance

So maybe you missed Bob Dylan’s infamous switch to electric at the Newport Folk Festival in 1965. These days, you, too, can go electric—with an electromechanical system instead of hydraulic. Our new e-book helps you overcome pre-conceived notions and provides tips for a successful performance.  

Comments (0)
Number of views (1571)
Article rating: No rating

Posted by Matt Gulleen on Di, Mai 04 2021 @ 9:30

Machine builders: Have it your way

Modified and custom actuators are another tool in your actuator design toolbox.

It’s usually straightforward to tweak a feature on a catalog product into something we call a modified standard product. Sometimes, you may need a highly customized solution for a specific application. That means starting with a blank sheet of paper. It all depends on your application and how the actuator is used in it. 

Comments (0)
Number of views (1301)
Article rating: No rating

Posted by Andrew Zaske on Di, Apr 06 2021 @ 9:16

Pneumatic rodless cylinders: Point-to-point motion control

Rodless cylinder technology is the basis of the subsequent generation of rodless pneumatic and today’s electric actuators

Rodless cylinder technology has evolved from the first band cylinder, introduced in 1955, to today's high-performance rodless electric actuators.

Comments (0)
Number of views (1429)
Article rating: No rating

Posted by Ryan Klemetson on Di, Mrz 02 2021 @ 9:30

How accurate is an actuator?

Do you want to hit the bulls-eye, or the same spot over and over?

Accuracy and repeatability are two separate but related concepts of a linear motion system. The motor, drive and electric actuator itself all influence accuracy and repeatability. It’s quite possible you may need repeatability more than accuracy.

Comments (0)
Number of views (2619)
Article rating: No rating

Posted by Andrew Zaske on Di, Feb 02 2021 @ 9:30

Fast and flexible: How to design a mask-making machine

Responding to the need for PPE for medical personnel

Manufacturer rapidly invents a new way to make face masks in response to the COVID-19 pandemic. Electric actuators assist with linear motion technology. 

Comments (0)
Number of views (1914)
Article rating: No rating

Posted by Andrew Zaske on Di, Dez 15 2020 @ 9:30

The best things come in sturdy packages

A wrap-up of how linear actuators are used to make boxes.

Automatic packaging machines must efficiently and consistently form and assemble boxes of all shapes and sizes. Pneumatic cylinders have been a long-standing and economcial solution for box-forming machines. However, electric linear actuators provide controlled movement and reliability advantages while meeting the same motion and force requirements.

Comments (0)
Number of views (1841)
Article rating: No rating
12345678910Last