Yes, extra cable can be ordered for the cylinder by adding a XA or XB to the end of the configuration string followed the desired length in inches. XA refers to the amount of extra cable on side 1, and XB for side 2.
Example: if a CC20 SK20 with a 2” auto tensioner (HK) and 10 inches of extra cable on the same side as the auto tensioner is required, the configuration string would be as follows.
CC20 SK20.000 HK-- XA10.000