Information and a procedure for using the CMF Import Tool
The Rockwell software will need a custom motor file (.cmf) to pair the Allen Bradley drive with the actuator properly. This file is also created by Allen Bradley. There are three ways to get this file, one is within the RSLogix 5000 V22 or newer Motor Database, a second is through the Rockwell Automation’s Knowledgebase library, and the other is to obtain it through Tolomatic and Allen Bradley, using the CMF Import Tool to install on the latter two.

Kontakt zu einem Ingenieur