Posted by Anonym on Tue, Oct 13 2015 @ 8:30 AM

Electric linear actuators and motors. Getting the right fit.

An electric linear actuator can outperform a pneumatic model with superior control of speed, position, and force as well as provide better accuracy and repeatability. But that superior performance comes with complexity. Pneumatic cylinders commonly are simple, easy-to-understand components, while electric linear actuators are systems comprised of a motor, controller, cables, and actuator. Plus attaching a motor to an actuator usually requires some kind of adaptor or housing.

Posted by Anonym on Tue, Sep 29 2015 @ 8:30 AM

Electric linear actuators deliver precise positioning for aerospace welding

Precision is integral to the aerospace and defense industries. Even a seemingly insignificant element of a device may be mission-critical, requiring the tightest manufacturing tolerances. That’s why when a rocket manufacturer contacted us about electric linear actuators that could hold their fuselage components in place for welding, we knew precise positioning would be a requirement.

Posted by Gary Rosengren on Tue, Sep 15 2015 @ 8:30 AM

[INFOGRAPHIC] Accuracy and repeatability in linear actuators

Machine builders frequently ask us, “How accurate is this actuator?” The answer is more than a number found in the product’s specifications. The real-world answer is much more complex.

In the real world of manufacturing, a greater degree of accuracy can come with a higher price tag. Sometimes you just need repeatability in your application, and that can be less costly. We urge you to thoroughly study the requirements and parameters of each application before selecting an actuator. Understanding the specific needs of each application will help you avoid excess costs and design a system with the best overall value.

Posted by Anonym on Tue, Sep 01 2015 @ 8:30 AM

3 steps to simpler linear actuator selection with new website

Visit www.Tolomatic.com and you’ll see something new. Our site’s been redesigned with a fresh, contemporary look. But even more exciting is that we’ve reorganized the site with simpler linear actuator selection, specification, and ordering in mind. In fact, on our new website, it takes three clicks or less to get the information you want.

Posted by Anonym on Tue, Aug 18 2015 @ 8:30 AM

Electric linear actuator sizing software makes selection easier

Selecting the right electric linear actuator for the task doesn’t have to be complicated. Our sizing software gets you to the right fit faster. The process begins when you enter your project parameters in our web interface at sizeit.tolomatic.com.The software asks the right questions and walks you through the specifying process step by step so you get the electric rod actuator or rodless electromechanical actuator that suits your application.

Posted by Gary Rosengren on Tue, Aug 04 2015 @ 8:30 AM

Electric linear actuator selection tips: Consider the environment

When you’re faced with electric linear actuator selection, one of the early considerations has to be the industrial environment in which it will operate. Will there be dust? How much dust and what kind? Will there be moisture? Direct spray? High temperatures and pressures? Corrosive substances?

These factors affect the performance of an electric linear actuator and may point to the best type for an application.

Posted by Gary Rosengren on Tue, Jul 21 2015 @ 8:30 AM

Better welds with electric linear actuators for resistance welding robots

U.S. and European car manufacturers have long been convinced of the benefits of automation in their production facilities. Spot welding robots are common in their body production lines.

Automation and robotics offer advantages in cost savings and quality, but plants in India, China, and Southeast Asia have been slow to get on the bandwagon. Perhaps some plant managers see these production processes as too expensive or difficult to implement. Whatever the reason, that situation may be changing according to a Frost & Sullivan study described in an article on The Fabricator.com

Posted by Anonym on Tue, Jun 16 2015 @ 8:30 AM

Compact, integrated linear actuator helps the show go on

Ever have an application where you had space for a pneumatic cylinder but needed the precision, programmability, and low maintenance of an electric linear actuator? You needed a compact, precise, reliable linear actuator. Does such a product exist? Of course it does! Here's a case study about an application where an integrated actuator solved this problem.

Posted by Anonym on Wed, May 27 2015 @ 8:30 AM

About the pneumatic linear actuator

Who doesn’t love a classic? There are classic clothes - like t-shirts and pull-over sweaters. Classic building designs - like Greek Revival and Victorian. Even classic cars. Whether it’s a building, a car or a pair of jeans, there’s nothing like the time-tested design and reliability of a classic.

When it comes to industrial automation, the pneumatic linear actuator or pneumatic air cylinder is a leading example of time-tested reliability. Since 1955, we've been developing and manufacturing these dependable workhorses for industry

Posted by Anonym on Tue, May 05 2015 @ 8:30 AM

Electrical noise and linear actuators

Electrical noise is a common occurrence. Random fluctuations in electrical signals are known as noise, and if the amplitude of the fluctuations becomes high enough, the noise can interfere dramatically with the operation of industrial automation devices like linear actuators.  The results can be anything from erratic movements to complete system failure.

First6789101112131415