Posted by Anonym on Tue, Oct 25 2016 @ 8:30 AM

Choosing the right linear actuator [INFOGRAPHIC]

When your design calls for a linear actuator, you have lots of choices.  Pneumatic, electric, rodless, rod, belt driven, screw driven. These are just some of the options available. 

Comments (0)
Number of views (1824)
Article rating: No rating

Posted by Anonym on Tue, Oct 04 2016 @ 8:30 AM

High force linear actuator: electric replaces hydraulic

It used to be that when a machine designer was confronted with a high force linear actuator application, the only solution was a hydraulic cylinder.  That meant the designer had to factor in the bulky hydraulic power unit (HPU), the inevitable leaks of hydraulic fluid and the downtime produced by frequent maintenance.

Now there’s another option when a high force linear actuator is needed. There are electric linear actuator products that can meet demanding specifications with ease. 

Comments (0)
Number of views (1682)
Article rating: No rating

Posted by Gary Rosengren on Tue, Sep 20 2016 @ 8:30 AM

Electric linear actuator accuracy and repeatability webinar

When an engineer is developing a machine design, accuracy is often top-of-mind.  So is machine cost. But these two considerations can be at odds since the usual scenario is that the higher the accuracy of a device, the higher the cost. This certainly holds true for electric linear actuators and linear motion systems.

Comments (0)
Number of views (1510)
Article rating: No rating

Posted by Anonym on Wed, Sep 07 2016 @ 8:30 AM

Electric linear actuators meet the challenge of FSMA

The federal Food Safety Modernization Act (FSMA) that was enacted in 2011 has energized the food industry around food safety and the prevention of food-borne illnesses. Most of the major producers and food equipment manufacturers have kept ahead of FSMA requirements successfully since food safety and prevention have always been among their top priorities.

Comments (0)
Number of views (1638)
Article rating: No rating

Posted by Anonym on Tue, Aug 23 2016 @ 8:30 AM

High force linear actuators: hydraulic vs roller screw actuators

How to select the best high force linear actuator for your application

Hydraulic cylinders have long been a leading choice for factory automation equipment needing a high force linear actuator. However, there have been advances in electric actuation (for example, the availability of roller screw actuators) which make these electric actuators suitable now for many high force applications.

Comments (0)
Number of views (2177)
Article rating: No rating

Posted by Anonym on Tue, Aug 09 2016 @ 8:30 AM

Electric actuator life in units of time: ball & roller screw actuators

A machine’s useful life depends on the life of its critical components. And machine designers  frequently hear the question, “How long can I expect this machine to keep working?”

When electric linear actuators are used, calculating life can be straight-forward for ball screw and roller screw actuators.  Since these screw types incorporate rolling elements as essential parts, you can use the L10 life formula for ball bearings.

Comments (0)
Number of views (1414)
Article rating: No rating

Posted by Anonym on Tue, Jul 26 2016 @ 8:30 AM

Solid-bearing, belt-driven linear actuator handles harsh environment

Many applications call for the carrying action of a rodless electromechanical actuator. And many of these need the high speed and long stroke capabilities of a belt-driven linear actuator. But what do you do when your application is in a dusty, harsh environment? Many rodless electromechanical actuators can’t handle these conditions. Their roller bearings get clogged with dust and stop working. Could a solid bearing be the solution?

Comments (0)
Number of views (1293)
Article rating: No rating

Posted by igor Glikin on Tue, Jul 12 2016 @ 8:30 AM

Selecting a rodless electromechanical actuator: belt- vs. screw-driven

Let’s say you’ve decided you need a rodless electromechanical actuator to carry a load in your application. Now you have to select a linear drive system. The two most common choices are screw drives and belt drives. Both drive types offer long life, low maintenance, and efficiency in converting the motor’s rotary motion to the carrier’s linear motion. However, each drive type is more suited to particular applications than others, depending on a few key factors.

Comments (0)
Number of views (1807)
Article rating: No rating

Posted by Anonym on Tue, Jun 28 2016 @ 8:30 AM

Electric linear actuator is clean-in-place, washdown ready

Stringent regulations govern the food processing industry. Food processing equipment and components, like electric linear actuators, must meet food safety regulations and stand up to clean-in-place (CIP) procedures. Food industry cleaning procedures may include regular washdowns with hot water, steam, high pressures, and caustic chemicals. Corrosion resistant materials and a water-shedding design are musts.

Comments (0)
Number of views (1103)
Article rating: No rating

Posted by Anonym on Tue, Jun 14 2016 @ 8:30 AM

Linear actuator helps convert conveyor to electric

Every factory relies on some kind of conveyor system to take components, work pieces, or finished goods from one place to another. In fact, most factories have several conveying systems, each tailored to a specific need. Conveying equipment is varied and essential. Components in these systems, like linear actuators, must be able to meet these varied needs and provide reliable performance.

Comments (0)
Number of views (1122)
Article rating: No rating
First6789101112131415