Show Mobile Nav

Posted by Aaron Dietrich on Thu, Apr 23 2015 @ 8:30 AM

Linear actuator reduces energy use in food & beverage processing

Once upon a time, managers of food and beverage processing plants considered energy costs to be a basic cost of doing business – something out of their control. But several factors have changed that attitude. Among them are rising energy prices, a challenging economy and an emphasis on reducing the environmental impact of manufacturing facilities.

Processors now see energy use as a cost that can and should be strategically managed. Companies are trying to optimize their energy budgets – increasing their plants’ energy efficiency, reducing use and looking for lower cost, cleaner energy sources. They're also looking at the energy use of all machinery and automation components like linear actuators.

Comments (0)
Number of views (132)
Article rating: No rating

Posted by Aaron Dietrich on Tue, Apr 07 2015 @ 8:30 AM

What you need to know about electric linear actuators

Electric or pneumatic? That is the question. Or at least it’s a crucial question that control systems and machine design engineers ask early in the process of specifying a linear actuator. A pneumatic cylinder may be the best solution -- easy-to-understand, lower cost -- but then again an electric linear actuator can offer distinct advantages. It really depends on the application.

Comments (0)
Number of views (157)
Article rating: No rating

Posted by Ryan Klemetson on Tue, Mar 24 2015 @ 8:30 AM

Brushless servo motors – more control for valves with linear actuators

Process industry engineers are looking to more sophisticated motion control solutions for valve automation because of an ever-growing need to improve productivity, increase efficiency, and minimize downtime.

These engineers must control the valves that regulate the flow of materials throughout a facility, and there are two basic ways to control these valves: linear motion (rising stem) and rotary motion (half turn or quarter turn). Powered rising stem valves are often used in mission-critical areas of a process. In these applications, reliability, repeatability, accuracy, and responsiveness are crucially important. These factors impact the type of valve actuation specified. There are traditional methods: pneumatic or hydraulic actuated systems and electric linear actuators driven by brush servo motors. Then there’s an emerging technology: brushless servo motor driven electric valve actuators.

Comments (0)
Number of views (408)
Article rating: No rating