Posted by igor Glikin on Tue, Jul 12 2016 @ 8:30 AM

Selecting a rodless electromechanical actuator: belt- vs. screw-driven

Let’s say you’ve decided you need a rodless electromechanical actuator to carry a load in your application. Now you have to select a linear drive system. The two most common choices are screw drives and belt drives. Both drive types offer long life, low maintenance, and efficiency in converting the motor’s rotary motion to the carrier’s linear motion. However, each drive type is more suited to particular applications than others, depending on a few key factors.

Comments (0)
Number of views (1365)
Article rating: No rating

Posted by Nick Holmgard on Tue, Jun 28 2016 @ 8:30 AM

Electric linear actuator is clean-in-place, washdown ready

Stringent regulations govern the food processing industry. Food processing equipment and components, like electric linear actuators, must meet food safety regulations and stand up to clean-in-place (CIP) procedures. Food industry cleaning procedures may include regular washdowns with hot water, steam, high pressures, and caustic chemicals. Corrosion resistant materials and a water-shedding design are musts.

Comments (0)
Number of views (709)
Article rating: No rating

Posted by Nick Holmgard on Tue, Jun 14 2016 @ 8:30 AM

Linear actuator helps convert conveyor to electric

Every factory relies on some kind of conveyor system to take components, work pieces, or finished goods from one place to another. In fact, most factories have several conveying systems, each tailored to a specific need. Conveying equipment is varied and essential. Components in these systems, like linear actuators, must be able to meet these varied needs and provide reliable performance.

Comments (0)
Number of views (692)
Article rating: No rating

Posted by Aaron Dietrich on Wed, Jun 01 2016 @ 8:30 AM

“How long will this actuator last?”

“How long will it last?” Every machine design engineer gets asked this question and will have to calculate the anticipated life of the machine – life that’s based on machine components including linear actuators. Engineers also have to consider expected life when they’re evaluating competing components.

Comments (0)
Number of views (1658)
Article rating: No rating

Posted by Aaron Dietrich on Tue, May 17 2016 @ 8:30 AM

Hydraulic linear actuator advantages and disadvantages

Hydraulic cylinders are popular automation components in many industries. Like other types of linear actuator (pneumatic and electric), they are used to move loads in a straight line. A hydraulic actuator uses the energy in a pressurized liquid, usually oil, to achieve this linear motion, as opposed to compressed air (pneumatics) or electricity.

Comments (0)
Number of views (4310)
Article rating: No rating

Posted by Nick Holmgard on Tue, May 03 2016 @ 8:30 AM

Webinar: tips on electric rod actuator selection

When you’re called on to specify electric linear actuators, one of the critical decisions you’ll face is whether to use a rodless or rod-style model. Either actuator type has advantages and disadvantages.

In general, if the actuator has to carry a load, a rodless product is what you need.  However, if a load needs to be pushed or pulled, select a rod-style actuator. 

Comments (0)
Number of views (801)
Article rating: No rating

Posted by Nick Holmgard on Tue, Apr 19 2016 @ 8:30 AM

Hygienic linear actuator keeps it clean

The world of food production and packaging is broad, varied and ever-changing. That world needs filling machines as diverse as the range of food products they process. Some filling machines have to handle powders and dry solids while others must handle thin or thick liquids. Some machines fill to a specified level, and some fill by volume or weight. This wide variety of equipment has a unifying need, though -- a need for hygienic design that can keep food products uncontaminated and withstand even the most stringent cleaning procedures.

Comments (0)
Number of views (665)
Article rating: No rating

Posted by Aaron Dietrich on Tue, Apr 05 2016 @ 8:30 AM

Linear actuators help prevent food contamination

How FSMA affects linear actuator selection

Until recently, the food processing industry has handled contamination reactively. If a foodborne illness was traced back to contamination at a manufacturing plant, the FDA (Food and Drug Administration) had the manufacturer fix the problem.

The flaw in this system, though, was that most of these illnesses were preventable. The Centers for Disease Control and Prevention estimates that 48 million people (1 in 6 Americans) get sick, 128,000 are hospitalized, and 3,000 die each year from foodborne diseases. That makes food contamination a major public health issue.

The federal government stepped in to change the way the FDA and food producers operate with the Food Safety Modernization Act (FSMA) – signed into law in January 2011. This important legislation shifts the focus to preventing contamination problems instead of just responding to them.  FSMA affects all automation components used in the industry, including linear actuators.

Comments (0)
Number of views (649)
Article rating: No rating

Posted by Aaron Dietrich on Tue, Mar 22 2016 @ 8:30 AM

Calculating total cost of linear actuators [INFOGRAPHIC]

Not too long ago many machine designers only considered the purchase price of automation components, like linear actuators, when they analyzed cost. And manufacturing management only looked at acquisition cost when they considered investing in automation.

Now machine designers and manufacturers are using a more thorough approach to cost analysis. Rather than looking at purchase price alone, they are looking into the “total cost of ownership” of a component, machine or technology. It's a business finance concept, used frequently when considering computer system upgrades.

Comments (0)
Number of views (948)
Article rating: No rating
12345678