Show Mobile Nav

Posted by Aaron Dietrich on Tue, Sep 12 2017 @ 8:30 AM

10 tips for specifying electric rod actuators: Part 1

(to be continued…)

There are lots of good reasons for specifying an electric rod actuator. Electric linear actuators offer a high degree of control over application parameters like position, velocity, and force. They deliver high degrees of accuracy and repeatability and can handle complex motion profiles.  All things considered, an electric rod actuator is often a superior actuation choice compared to pneumatic or hydraulic cylinders.

Comments (0)
Number of views (1056)
Article rating: No rating

Posted by Aaron Dietrich on Wed, Sep 06 2017 @ 8:30 AM

Supporting STEM education

Science, technology, engineering, and mathematics (together known as STEM) impart valuable life skills.  STEM subjects teach students how to gather and evaluate evidence, make sense of information, and use new insights and knowledge to find solutions to complex problems.

Comments (0)
Number of views (816)
Article rating: No rating

Posted by Aaron Dietrich on Tue, Aug 22 2017 @ 8:30 AM

How to select electric linear actuators that stand the test of time

The length of time a linear actuator will function (i.e., service life) is critically important to a machine designer. Machines need to keep working reliably with little or no need for lengthy maintenance that will take a machine off-line . So, components like actuators must keep working.

Comments (0)
Number of views (1251)
Article rating: No rating

Posted by Aaron Dietrich on Tue, Aug 08 2017 @ 8:30 AM

Electric high force linear actuator is tough enough to process lumber

The lumber industry has relied on the toughness and high force capabilities of hydraulic cylinders for years.  But lately that reliance has been shaken.  Hydraulic cylinders leak and can contaminate the fragile eco-systems in which lumber processing operates.  Plus, hydraulic systems are only 40-55% efficient and cylinders require frequent maintenance.  When combined, these factors can make hydraulic cylinders an expensive choice in the long run.

The introduction of electric high force linear actuators has given the lumber industry a new option for linear motion.

Comments (0)
Number of views (2273)
Article rating: No rating

Posted by Aaron Dietrich on Tue, Jul 25 2017 @ 8:30 AM

Total cost of ownership: pneumatic vs electric linear actuators

[WEBINAR]

Who doesn’t like to save money?  We’re all in search of a good deal, but how do you define what’s good?  If you buy something on the cheap but it falls apart in a short time, is that a good deal?  Maybe it’s smarter to pay more for something that last longer and performs better.

In business, this means considering total cost of ownership (TCO), that is, initial acquisition cost plus operating costs. Comparing TCO to purchase price alone is especially interesting when applied to pneumatic and electric linear actuators. 

Comments (0)
Number of views (1009)
Article rating: No rating

Posted by Nick Holmgard on Tue, Jul 11 2017 @ 8:30 AM

Electric cylinders essential to advanced conveyor system [Case Study]

Conveying systems are common in manufacturing. They can be straight-forward systems that take packages from point A to point B or complex ones for sorting and diverting.  Systems used in food processing also must handle washdowns, a common practice in the industry.

As critical components, linear actuators must withstand the challenges of the application including environmental ones.  Pneumatic cylinders have been used extensively in conveying. However, electric cylinder use is growing, fueled by demand for programmability and better accuracy.

Comments (0)
Number of views (1143)
Article rating: No rating

Posted by Aaron Dietrich on Tue, Jun 27 2017 @ 8:30 AM

High force linear actuators – hydraulic vs electric [WEBINAR]

When your application calls for a high force linear actuator, you may believe that your only choice is a hydraulic cylinder.  Hydraulics have long been the leading choice for automation equipment needing high force. However, now there are electric high force linear actuators  that offer important advantages over hydraulics in terms of performance and total cost of ownership.  Watch this webinar, and you may want to reconsider the merits of using an electric rod actuator.

Comments (0)
Number of views (1273)
Article rating: No rating

Posted by Gary Rosengren on Tue, Jun 13 2017 @ 8:30 AM

Which is best for high force linear actuators: Ball or roller screws?

If you’re selecting an electric high force linear actuator, you may believe you know the answer to the question in the headline.  The force transmission prowess of roller screws is well known.  But before you go to the expense of a roller screw linear actuator, take a careful look at the application.  You may find that a ball screw actuator will do the job.  And that could mean significant savings.

Comments (0)
Number of views (952)
Article rating: No rating

Posted by Gary Rosengren on Wed, May 31 2017 @ 8:30 AM

How to specify an electric linear actuator that’s industrial strength

Manufacturing environments can be challenging.  There may be dust or metal shavings.  There may be oil, coolant, or water. There may be corrosive agents like solvents, cleaners, and various chemicals and compounds.

All these factors impact the performance and life of components like electric linear actuators.  Dust may clog the action or cause parts to wear out prematurely.  Moisture may short electrical connections and cause rusting.  Corrosive agents can eat away at housings, seals, fasteners, and more. Industrial environments call for industrial strength components.

A machine designer needs confirmation that a component will stand up to environmental factors.

Comments (0)
Number of views (1254)
Article rating: No rating

Posted by Nick Holmgard on Tue, May 16 2017 @ 8:30 AM

Electric rod actuator cleans up after hydraulics

Hydraulic cylinders are well-known linear motion workhorses in industrial machinery.   They’re reliable, familiar, capable of high force, and affordable, but they’re not without disadvantages. The leading ones are fluid leaks, large footprint (with hydraulic power unit or HPU), cumbersome changeovers due to lack of programmability, and high maintenance costs.

The introduction of electric high force linear actuators means machine designers now have a choice. An electric rod actuator can replace a hydraulic cylinder and eliminate the need to clean up leaks.

Comments (0)
Number of views (560)
Article rating: No rating
12345678