Posted by Aaron Dietrich on Tue, Jan 10 2017 @ 8:30 AM

Ball and roller screw linear actuators: How to compare service life

When you’re designing equipment, you'll probably be asked, “How long will this machine last?” And even if you’re not asked outright, you know service life is an essential consideration. It’s a critical factor you consider when sourcing components.

Electric linear actuators are important components in many machines, and the “how long will it last” question is a familiar one. If it’s a ball or roller screw actuator, you can use a formula to help estimate life based on load – the same formula used to estimate bearing life. 

Comments (0)
Number of views (874)
Article rating: No rating

Posted by Aaron Dietrich on Tue, Aug 09 2016 @ 8:30 AM

Electric actuator life in units of time: ball & roller screw actuators

A machine’s useful life depends on the life of its critical components. And machine designers  frequently hear the question, “How long can I expect this machine to keep working?”

When electric linear actuators are used, calculating life can be straight-forward for ball screw and roller screw actuators.  Since these screw types incorporate rolling elements as essential parts, you can use the L10 life formula for ball bearings.

Comments (0)
Number of views (718)
Article rating: No rating

Posted by Aaron Dietrich on Wed, Jun 01 2016 @ 8:30 AM

“How long will this actuator last?”

“How long will it last?” Every machine design engineer gets asked this question and will have to calculate the anticipated life of the machine – life that’s based on machine components including linear actuators. Engineers also have to consider expected life when they’re evaluating competing components.

Comments (0)
Number of views (1658)
Article rating: No rating