Show Mobile Nav

Posted by Aaron Dietrich on Tuesday, January 9, 2018

Selection tips: rodless electromechanical & electric rod actuators

electric linear actuator groupWhen you specify a linear actuator, some basic decisions come first. Like electric or fluid-powered? Like do you need the push/pull of an electric rod actuator or the load-carrying action of a rodless electromechanical actuator?

We’ve compiled tips for selecting these actuator types.  Here’s an opportunity to increase your knowledge of electric linear motion with two white papers: How to specify electric rod-style actuators for optimal performance, reliability and efficiency and Specifying electric rodless actuators: Ten tips for maximizing actuator life and system performance. Download them here.


Selection tips for electric linear actuators

Rod-style or rodless, here are tips for specifying the right electric motion solution for the task.

  1. Calculate size for electric, not fluid power  Don’t fall into the common fluid power practice of oversizing. Fluid-powelectric actuator sizing softwareered actuators can be low cost, so a bigger cylinder won’t blow the budget. In comparison, electric actuators have higher purchase prices, so oversizing can be costly. Use sizing software offered by manufacturers to get the right size linear actuator for your application. 
  2. Calculate loads precisely  If you know the weight and size of the load, how far it needs to travel and how fast it needs to move, you can accurately specify actuator components, like screws, bearings and motors. Accurately-specified components mean longer service life for the linear actuator. 
  3. Factor in the duty cycle  Duty cycle for a linear actuator is the ratio of operating time to resting time. It’s expressed as a percentage. Knowing the duty cycle means you can specify an actuator that will last.
  4. Set critical speed limits  Actuator lead screws have critical speed limits. If the screw has to operate at or beyond its limit, it will oscillate, causing noise and vibration. Long-term effects could be premature wear and even catastrophic failure. 
  5. Factor in the environment  Moisture, dust and corrosive agents can cause problems for linear actuators. If a linear actuator is in a washdown environment, there are special issues to consider. food processing washdown
  6. Look beyond footprint when specifying a drive system  Reverse parallel motor mounting has the appeal of saving space, but the fact that power is transmitted through belts or gears means these configurations are less power and efficiency. Sometimes only an inline motor configuration delivers the speed and thrust required. 
  7. Match actuator capabilities to life expectations  An electric linear actuator will fail if its drive or carrier bearing system is over-stressed by load and speed. For long service life, specify an actuator that’s suited to the task. 


Special tips foelectric linear motionr electric rod actuators

Because an electric rod actuator pushes or pulls its load, there are two special considerations to keep in mind when specifying this type of actuator.

  1. Avoid side loading  Electric rod actuators do not support the load, so the load’s weight can deflect the rod and cause wear on seals and bearings as well as accuracy problems.

  2. Keep total envelope size in mind  Since the rod extends beyond the actuator body, the total footprint will be the actuator length plus the stroke length.


Special tips for rodless electromechanical actuators  

A rodless electromechanical actuator carries its load and is subject to different stresses than its rod-style counterparts. Here are two tips for specifying rodless actuators.rodless electromechanical actuator

  1. Calculate all moments (torques)  Since rodless electromechanical linear actuators carry loads, the load-carrying platform will be stressed. You can only specify the right actuator for an application if you’ve calculated carrier roll, yaw and pitch.
  2. Mounting makes a difference  Mounting is always critical but especially for a long-stroke rodless linear actuator. You’ll need enough support points to ensure rigidity. Also, you’ll need a mounting surface that’s straight and flat, plus room for the actuator/motor combination.

Tolomatic has broad offerings of both rod-style and rodless actuators, so we can help you find the best electric linear motion solution for your application.


Learn more

For tips on selecting electric linear actuators, down our white papers: How to specify electric rod-style actuators for optimal performance, reliability and efficiency and Specifying electric rodless actuators: Ten tips for maximizing actuator life and system performance.

Interested in electric linear motion? Join the discussion at our LinkedIn group.

Please login or register to post comments.