Home  >  Pneumatic Actuators  >  Pneumatic Rodless  >  Band Cylinders™ and Slides  >  MXP Cylinders

Carrier Adjustments

MX_S- Solid Bearing Carrier Bracket Adjustment

The S-Solid bearing carrier will provide for maximum life when properly adjusted. The carrier design contains both tension and lock screws. The tension screws control the amount of pressure placed on the carrier bearings. The lock screws lock the tension screws in place and provide fine adjustment of the carrier bearings. The number of tension and lock screws will vary depending on the bore size of the actuator.

Carrier Adjustment Procedures

  1. Fully loosen all tension and lock screws. They do not need to be removed, just fully loosened.
  2. Tighten tension screws on both sides of carrier roughly 1/8 to 1/4 turn clockwise past where the screw starts to feel snug. The carrier should be very difficult or impossible to move by hand.
  3. Next, adjust the lock screws on both sides of the carrier roughly 1/8 to 1/4 turn clockwise past where the screw starts to engage.
  4. Ideal carrier tension is achieved when the carrier feels snug in relation to the tube. No rocking motion should be present. The carrier should be loose enough to be moved by hand over the entire length of the actuator. If after this process the carrier has become too loose, equally adjust all of the lock screws with a slight 1/32 turn counter-clockwise. A carrier that is adjusted too tight will increase the breakaway pressure required for motion; in extreme cases no motion will occur when air is applied.

During the service life, this process may need to be repeated. Keeping the carrier properly adjusted will prolong the life of the S-Solid bearing system.

Watch the MX S- Solid Bearing Carrier Adjustment Procedure.

MX_16S
cautionSymbol.gif
NOTE: MX_16S requires a different carrier adjustment procedure, see below.
S-bearingAdjMX_16.gif
Tools Required:
Inch Models: 1/16 inch and 2.5mm Hex Wrench (Key)
Metric Models: 2 and 2.5 mm Hex Wrench (Key)
  1. Loosen endplate screws on both ends of the carrier.
  2. Fully loosen all tension and lock screws. They do not need to be removed, just fully loosened.
  3. Tighten tension screws by turning them clockwise until the carrier is just tight enough so that no side-to-side rocking motion is present and it can easily be moved by hand over the entire stroke length with no hesitation. Very little torque on the screws is required to obtain this condition.
    Note: The Tension Screws are the small set screw style fastener. The Lock Screws are the larger, low head, hex drive screws.
  4. Tighten lock screws by turning them clockwise until tight. The carrier should feel snug in relation to the tube, with no side-to-side rocking motion present. If the carrier becomes too loose, loosen the lock screws, tighten the tension screws and then retighten the lock screws.
  5. Once ideal carrier tension is achieved, fully tighten end plate screws on both ends of the carrier.

Allen wrench sizes for carrier adjustment, Solid bearing actuators
  Tension Screw Lock Screw
  in mm in mm
16  1/16
 2
 1/16
 2
25  5/32
 4
 1/8
 3
32  5/32
 4
 3/32
 2
40  5/32
 4
 1/8
 3
50  3/16
 4
 3/32
 2.5
63  1/4
 5
 3/16
 5