Radial Load
|
Regeneration
|
Regeneration braking
|
Repeatability
|
Repeatability & accuracy
|
Resolution
|
Resolver
|
Reverse radial load
|
RMS Torque
|
RS232
|
| |
| Radial Load |
| Load where the force is acting perpendicular to the axis of actuator (bearing) in the direction of actuator (bearing). |
| back to top |
| |
| Regeneration |
| Characteristic of a motor to act as a generator when the CEMF (counter electromotive force) is larger than the drive’s applied voltage. |
| back to top |
| |
| Regeneration braking |
| The technique of slowing or stopping a drive by regeneration. |
| back to top |
| |
| Repeatability |
The degree to which an actuator can return to a reference location. Notice on the bullseye on the next page that the holes are close together, however the grouping is far from the bullseye. Repeatability can be thought of as how tight of a grouping can be made. Unidirectional repeatability, measured by approaching a position from a single direction, hides errors caused by backlash and hysteresis effects. Bidirectional repeatability, measured by approaching a position from opposing directions, includes these effects, and provides a more meaningful specification.
 |
| back to top |
| |
| Repeatability & accuracy |
The measure of how close to a programmed point the actuator can come, and how close it gets to that same point again. The repeatability of industrial actuators is usually much better than the accuracy. Notice on the bullseye below that the points are centered around the middle of the target and are grouped close together. This is good accuracy and repeatability.
 |
| back to top |
| |
| Resolution |
| The smallest position increment that can be achieved. |
| back to top |
| |
| Resolver |
| A feedback device consisting of a stator and rotor that provides position and velocity information to the drive for commutation. |
| back to top |
| |
| Reverse radial load |
| Load where the force is acting perpendicular to the axis of actuator (bearing) in the direction opposite from actuator (bearing). |
| back to top |
| |
| RMS Torque |
| In an intermittent application, this is the torque provided to generate equivalent motor heating to one operating in a steady state.
Trms=
where: Ti= Torque during interval i
ti= Time of interval i |
| back to top |
| |
| RS232 |
| A standard for data communication that defines voltages and time requirements for information to be transferred on a single line in sequential format. |
| back to top |
| |