Parallel Port
|
Piston
|
Port
|
Pounds Per Square Inch
|
Proximity Sensor
|
Pulley
|
| |
| Parallel Port |
| Metric versions of the BC2, BC3, BC4 and LS have the choice of parallel port and taper port. |
| back to top |
| |
| Piston |
| A sliding component moved by fluid pressure. It usually consists of a short, solid metal cylinder within a cylindrical vessel in which it moves back and forth. |
| back to top |
| |
| Port |
| In pneumatic units, the area to make connection to air lines that supply power to the actuator. In electrical units: a connecting unit between a data link and a device. |
| back to top |
| |
| Pounds Per Square Inch |
| A measurement of pressure in the American system. By way of comparison, the weight of the atmosphere (one atmosphere) is 14.7 pounds per square inch, at sea level. It is used to express pressure in both pneumatic and hydraulic-powered systems. In the IS Metric system, pressure is measured in Bars. To covert PSI to Bars, take the PSI figure and multiply it by 0.0689476. |
| back to top |
| |
| Proximity Sensor |
| An LED-equipped device for sensing end-of-stroke on cylinder slides. Proximity sensors supply either a sourcing signal or a sinking signal to a device such as a programmable logic controller. |
| back to top |
| |
| Pulley |
| A sheave or small wheel with a grooved rim used with a cable cylinder to change the direction and point of application of the pulling force generated by the cylinder’s piston. |
| back to top |
| |