Home  >  Glossary

Glossary Terms

Pneumatic Actuators
Rodless pneumatic actuators and rod cylinder slides
  
Click a letter to view terms starting with that letter:

ALL A B C D E F G H I J K L M N O P Q R S T U V W X Y Z


Dead length
Deflection
Dead length
Deceleration
Deflection
Die-Cast
Double-Acting Cable Cylinder
Double-Purchase cable Cylinder
Dual 180 Carrier
Dual Magnet
Dust Band
  
Dead length
Result of subtraction of stroke length from overall length of an actuator.
back to top
  
Deflection
Amount of displacement of a point on rodless actuator carrier or rod actuator tooling plate, under load by forces or bending moments, measured in the direction perpendicular to actuator axis.
back to top
  
Dead length
Dead length is the part of the band cylinder or linear slide required for mounting and mechanisms. The overall length of a band cylinder or linear slide is the stroke length plus the dead length.
back to top
  
Deceleration
The opposite of acceleration. Deceleration means diminished velocity or slowing down.
back to top
  
Deflection
A measurement of the amount of bend under the weight of a load, such as that to which a load-supporting rod or cable is subject.
back to top
  
Die-Cast
A metal-forming process similar to injection-molding for plastic. In Die-Casting, molten metal (usually aluminum) is injected into a mold under pressure.
back to top
  
Double-Acting Cable Cylinder
Cable cylinder that applies equal force in two directions.
back to top
  
Double-Purchase cable Cylinder
Cable cylinder that uses additional cable and pulleys to double the velocity and stroke of cable cylinders.
back to top
  
Dual 180 Carrier
Option for the BC3 that gives greater bending moments without using a larger actuator.
back to top
  
Dual Magnet
Option for BC2 with two magnets, one on each side of the carrier.
back to top
  
Dust Band
Part of Tol-O-Matic’s patented band retention system, the external band.
back to top