Home  >  Glossary

Glossary Terms

Electric Linear Motion
Rodless screw and belt drive actuators, rod style screw and belt drive actuators, brushless servo motors and controls
  
Click a letter to view terms starting with that letter:

ALL A B C D E F G H I J K L M N O P Q R S T U V W X Y Z


Absolute Move
AC Servo
Accuracy
Acme Screw/Nut
Auto-phasing
Axial Loading
Actuator
Anodizing
Auxiliary Carrier
  
Absolute Move
A move with reference to a fixed absolute zero location.
back to top
  
AC Servo
Motor/Drive that generates sinusoidal motor currents and sinusoidal back EMF in a brushless motor.
back to top
  
Accuracy
The degree to which an actuator is able to move to a specific commanded point. On the bullseye below, notice that all the holes are centered around the middle of the target, but the grouping is not very close together. Good accuracy does not require good repeatability. (see repeatability & accuracy

back to top
  
Acme Screw/Nut
Threaded screw and nut design which utilizes sliding surfaces between the two. Typical efficiencies are between 60-70%.
back to top
  
Auto-phasing
The drive function that determines the motor’s angular rotor position for commutation without the need for Hall Effect switches.
back to top
  
Axial Loading
Load where the force is acting along the axis of actuator (bearing) in any direction.
back to top
  
Actuator
A mechanism for moving or controlling something indirectly instead of by hand.
back to top
  
Anodizing
Protective treatment for aluminum that involves subjecting the metal to electrolytic action in a chemical bath, to create a protective film of aluminum oxide with a very smooth finish.
back to top
  
Auxiliary Carrier
An option for band cylinders or linear slides that increases the load capacity of the cylinder as well as increasing the capacity of bending moment about the Y axis. Note: internal cushion will not work when auxiliary carrier ordered without piston, it will be necessary to add external shock absorbers.
back to top