Home  >  Glossary

Glossary Terms

Electric Linear Motion
Rodless screw and belt drive actuators, rod style screw and belt drive actuators, brushless servo motors and controls
  
Click a letter to view terms starting with that letter:

ALL A B C D E F G H I J K L M N O P Q R S T U V W X Y Z


Absolute Move
AC Servo
Accuracy
Acme Screw/Nut
Auto-phasing
Axial Loading
Back EMF
Backlash
Bending Moment
Dead length
Deflection
Duty Cycle
Dwell Time
Efficiency
Encoder
Flatness
Gantry
Holding Torque
Incremental move
Inertia
Inertia Match
Lead
Maximum static load
Repeatability & accuracy
Stepper Motor
Vector drive
Actuator
Auxiliary Carrier
Center of Gravity
Configurator
Configuration String
Hall-effect D.C. Switch
Inch-Pound
Anodizing
Tube Deflection
Units
Ball Screw/Nut
Baud Rate
Breakaway Torque
Brushless DC Servo
Carrier
Closed Loop (Feed Back)
Commutation
Continuous torque
Critical Speed
Cycle
Cycle Rate
Load
Maximum dynamic Load
Maximum dynamic Load
Microstepping
Moment Load
Motion Profile
Open Loop
Optically Isolated
Pitch
PLC
PWM
Radial Load
Regeneration
Regeneration braking
Repeatability
Resolution
Resolver
Reverse radial load
RMS Torque
RS232
Servo
Servo Motor
Slew
Stall Torque
Stiffness
Straightness
Stroke length
Thrust
Torque
Torque Constant
Voltage Constant
Trapezoidal Profile
Triangular Profile
  
Absolute Move
A move with reference to a fixed absolute zero location.
back to top
  
AC Servo
Motor/Drive that generates sinusoidal motor currents and sinusoidal back EMF in a brushless motor.
back to top
  
Accuracy
The degree to which an actuator is able to move to a specific commanded point. On the bullseye below, notice that all the holes are centered around the middle of the target, but the grouping is not very close together. Good accuracy does not require good repeatability. (see repeatability & accuracy

back to top
  
Acme Screw/Nut
Threaded screw and nut design which utilizes sliding surfaces between the two. Typical efficiencies are between 60-70%.
back to top
  
Auto-phasing
The drive function that determines the motor’s angular rotor position for commutation without the need for Hall Effect switches.
back to top
  
Axial Loading
Load where the force is acting along the axis of actuator (bearing) in any direction.
back to top
  
Back EMF
Voltage produced across a motor winding due to the winding turns being cut by a magnetic field. This voltage is directly proportional to rotor velocity and is opposite in polarity to the applied voltage.
back to top
  
Backlash
Linear distance which is lost in positioning the nut or carrier when the screw direction of rotation changes.
back to top
  
Bending Moment
Equivalent torque produced by a force displaced by a known distance from the carriage. Ex. Mx, My, Mz, Fz

back to top
  
Dead length
Result of subtraction of stroke length from overall length of an actuator.
back to top
  
Deflection
Amount of displacement of a point on rodless actuator carrier or rod actuator tooling plate, under load by forces or bending moments, measured in the direction perpendicular to actuator axis.
back to top
  
Duty Cycle
Ratio of on time to total cycle time. Duty Cycle = On Time (On Time + Off Time)
back to top
  
Dwell Time
A pause of motion within a move cycle.
back to top
  
Efficiency
Ratio of power output to power input.
back to top
  
Encoder
Device used to provide relative position and velocity information to a drive or controller by sensing mechanical motion and providing a corresponding pulse rate as output.
back to top
  
Flatness
When traveling in a straight horizontal line, the vertical deviation above or below the horizontal plane of travel of the carrier.
back to top
  
Gantry
A method of connecting two actuators together by a drive shaft so one motor can operate both actuators.
back to top
  
Holding Torque
Maximum external torque that can be applied to a stopped, energized motor without causing the rotor to rotate.
back to top
  
Incremental move
A positional move referenced from the current position.
back to top
  
Inertia
Measure of an object’s resistance to change in motion that is a function of the object’s mass and shape.
back to top
  
Inertia Match
If the reflected inertia of the load is equal to the rotor inertia of the motor, the system will operate optimally for efficiency and dynamic performance.
back to top
  
Lead
Linear travel of a lead screw nut or carriage for every one full rotation of the lead screw expressed in inches per rev.
back to top
  
Maximum static load
Maximum load of constant magnitude acting in one direction that a static actuator (component) can withstand without permanent deformation.
back to top
  
Repeatability & accuracy
The measure of how close to a programmed point the actuator can come, and how close it gets to that same point again. The repeatability of industrial actuators is usually much better than the accuracy. Notice on the bullseye below that the points are centered around the middle of the target and are grouped close together. This is good accuracy and repeatability.

back to top
  
Stepper Motor
Motor which translates electrical pulses into motion, where the pulse rate controls velocity and position.
back to top
  
Vector drive
A class of drives that sense motor current in each individual motor phase and resolves these readings into two current vectors. One vector is the torque producing current and other is the waste current. The current control algorithm then works to drive the non-torque-producing component to zero. This result in a high bandwidth torque response over the full speed range without the phase lag and tolerance issues that place older drive technologies.
back to top
  
Actuator
A mechanism for moving or controlling something indirectly instead of by hand.
back to top
  
Auxiliary Carrier
An option for band cylinders or linear slides that increases the load capacity of the cylinder as well as increasing the capacity of bending moment about the Y axis. Note: internal cushion will not work when auxiliary carrier ordered without piston, it will be necessary to add external shock absorbers.
back to top
  
Center of Gravity
(Center of Mass) The point a which the entire weight of a body may be considered as concentrated so that if supported at this point the body would remain in equilibrium in any position.
back to top
  
Configurator
Name given to the software that uses the configuration string to give instructions to the factory with correct specifications to create your built-to-order actuator.
back to top
  
Configuration String
A series of code letters and numbers that Tol-O-Matic uses to create built-to-order actuators.
back to top
  
Hall-effect D.C. Switch
A magnetically-controlled transistor switch controlling DC power. It has no moving parts and theoretically unlimited contact life.
back to top
  
Inch-Pound
A unit of measure of torque. It is derived from a given force in pounds acting at a given radius in inches (pounds multiplied by inches = inch-pounds). An inch-pound is 1/12th of a foot-pound. Inch-pounds may be converted to the IS Metric equivalent of Newton-meters by multiplying them by 0.1129848. Newton-meters may be converted to inch-pounds by multiplying them by 8.850748.
back to top
  
Anodizing
Protective treatment for aluminum that involves subjecting the metal to electrolytic action in a chemical bath, to create a protective film of aluminum oxide with a very smooth finish.
back to top
  
Tube Deflection
Due to the nature of loads and aluminum extrusions tube deflection will occur if cylinder (linear slide) is supported only on the ends without tube supports at recommended intervals along length of cylinder.
back to top
  
Units
U.S. Standard: A system of weights and measures based on the pound and inches. Metric: A decimal system of weights and measures based on the kilogram and meter.
back to top
  
Ball Screw/Nut
Screw and nut design utilizing a nut that contains one or more circuits of recirculating steel balls which roll between the screw and nut.
back to top
  
Baud Rate
Number of binary bits transmitted per second in a serial communication system.
back to top
  
Breakaway Torque
Torque required to start an actuator in motion. In an electric actuator, this consists primarily of the torque to overcome the preload of the lead screw nut assembly and the static friction of the carrier bearings.
back to top
  
Brushless DC Servo
Motor/drive that generates trapezoidal motor currents and trapezoidal back EMF in a brushless motor.
back to top
  
Carrier
Moving part of a rodless actuator providing a mounting surface for a load.
back to top
  
Closed Loop (Feed Back)
System where the output is measured and compared to the input. If this system is capable of making corrections to minimize the difference it is classified as a servo.
back to top
  
Commutation
Switching of drive voltage to the motor windings necessary to provide continuous rotation. A brush motor uses mechanical switching through a brush-bar contact. Brushless motors use separate devices such as Hall Sensors to sense the rotor position. This information is then processed by the drive to determine the switching sequence.
back to top
  
Continuous torque
Another term for RMS torque. See RMS torque
back to top
  
Critical Speed
Rotational speed of a lead screw at which the screw begins to oscillate or whip. This speed is dependent on the screw length and diameter.
back to top
  
Cycle
A complete motion of actuator’s carrier or tooling plate from start to finish and back.
back to top
  
Cycle Rate
Total number of complete cycles in a specific period of time.
back to top
  
Load
A mass or weight supported by the carrier (rodless cylinders) or tooling plate (rod type cylinders). Ex. Fz

back to top
  
Maximum dynamic Load
Load of constant magnitude acting in one direction that results in a nominal life (travel) of a linear motion actuator (component).
back to top
  
Maximum dynamic Load
Load of constant magnitude acting in one direction that results in a nominal life (travel) of a linear motion actuator (component).
back to top
  
Microstepping
Type of drive that proportions the current in a step motor’s windings to provide intermediate positions between full steps. Advantages over full and half stepping include smoothness of rotation and higher position resolution.
back to top
  
Moment Load
Rotational forces applied to the carrier equal to the linear force applied (weight) multiplied by the distance between the location of the force (center of gravity) and the surface center of the carrier. Typically expressed as yaw (Mz), pitch (Mx) and Roll (My). (See illustration with “LOAD”).
back to top
  
Motion Profile
Definition of an objects position and velocity relationships in time during a move.
back to top
  
Open Loop
Motion control system where no position or velocity signals are provided for correction. Typically, stepper systems run as open loop systems.
back to top
  
Optically Isolated
Transmission of a signal from one device to another with a light source (emitted) and sensor (received), in order to avoid direct electrical contact
back to top
  
Pitch
Number of revolutions required by a leadscrew to move the nut or carrier one inch, expressed in revs/per inch
back to top
  
PLC
(Programmable logic controller) A digital electronic device that uses to store instructions and to implement functions such as logic sequencing, timing and counting in order to control machines and processes.
back to top
  
PWM
Pulse Width Modulation is a method of controlling current in the windings of a motor by on-off switching of transistors to vary the duty cycle.
back to top
  
Radial Load
Load where the force is acting perpendicular to the axis of actuator (bearing) in the direction of actuator (bearing).
back to top
  
Regeneration
Characteristic of a motor to act as a generator when the CEMF (counter electromotive force) is larger than the drive’s applied voltage.
back to top
  
Regeneration braking
The technique of slowing or stopping a drive by regeneration.
back to top
  
Repeatability
The degree to which an actuator can return to a reference location. Notice on the bullseye on the next page that the holes are close together, however the grouping is far from the bullseye. Repeatability can be thought of as how tight of a grouping can be made. Unidirectional repeatability, measured by approaching a position from a single direction, hides errors caused by backlash and hysteresis effects. Bidirectional repeatability, measured by approaching a position from opposing directions, includes these effects, and provides a more meaningful specification.

back to top
  
Resolution
The smallest position increment that can be achieved.
back to top
  
Resolver
A feedback device consisting of a stator and rotor that provides position and velocity information to the drive for commutation.
back to top
  
Reverse radial load
Load where the force is acting perpendicular to the axis of actuator (bearing) in the direction opposite from actuator (bearing).
back to top
  
RMS Torque
In an intermittent application, this is the torque provided to generate equivalent motor heating to one operating in a steady state. Trms= where: Ti= Torque during interval i ti= Time of interval i
back to top
  
RS232
A standard for data communication that defines voltages and time requirements for information to be transferred on a single line in sequential format.
back to top
  
Servo
System that compares the output of a device (by monitoring position, velocity, and/or torque) with the desired outcome and makes corrections to minimize the difference.
back to top
  
Servo Motor
Motor used in closed loop systems where feedback is used to control motor position, velocity, and/or torque, usually expected to have high torque/inertia ratio.
back to top
  
Slew
Constant non-zero velocity portion of a motion profile.
back to top
  
Stall Torque
Maximum torque available at zero speed.
back to top
  
Stiffness
System ability to maintain accuracy when subject to disturbance.
back to top
  
Straightness
When traveling in a straight horizontal line, the side to side deviation within the horizontal plane of travel of the carrier.
back to top
  
Stroke length
The distance that the carrier and its load will move on the actuator.
back to top
  
Thrust
Measurement of linear force
back to top
  
Torque
Measurement of force producing rotation.
back to top
  
Torque Constant
Torque generated in a DC motor per ampere applied to the windings.
back to top
  
Voltage Constant
Back EMF generated by a DC motor usually in units of volts per 1000 rpm.
back to top
  
Trapezoidal Profile
A velocity vs time profile that is characterized by total move time spit evenly for acceleration, deceleration and velocity.
back to top
  
Triangular Profile
A velocity vs time profile that is characterized by equal time for acceleration and deceleration.
back to top